Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
I'm currently looking at implementing automatic testing using the OMAP-L138. I'm able to setup scripts that will execute only on the DSP or the ARM core, but when I go to execute on both using the simultaneous member of the server class, only the DSP will cleanly execute. The ARM execution produces the following error:
"ARM9_0: Can't Run Target CPU: (Error -2030 @ 0x52545441) Internal error: Access to unknown or invalid register was requested. Restart the application. If error persists, please report the error. (Emulation package 8.0.27.9)".
If the only change I make to the script is to comment out the entry for the DSP session in the DebugSession array assignment I pass to the simultaneous.run() function, the ARM core will execute without any issues.