This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS: ccs V9 and the C6713dsk

Intellectual 300 points

Replies: 2

Views: 231

Tool/software: Code Composer Studio

Thanks for the previous answer.

It's ok to use the lcdk with ccs v9. HOw ever, is there a way I can salvage my 50 C6713DSKs in the realm of ccsV9.

Thanks

Dan

U of S

  • Guru 335225 points

    Hello

    Daniel Gaucher
    HOw ever, is there a way I can salvage my 50 C6713DSKs in the realm of ccsV9.

    You will have to use an external debug probe attached to J8 of the DSK (see section 3.6.2 of the C6713DSK documentation). You will not be able to use the on-board debug probe since it is based off the obsolete XDS510USB, which is no longer supported by CCSv9.

    If you wish to use the on-board probe, you will have to stick with CCSv8.3.

    thanks

    ki

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training/Documentation? Check out the CCS Resources page

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

  • Guru 159155 points

    Dan,

    Hmm, that is a though scenario, especially due to the amount of boards you have. 

    You have two options:

    - Stay with CCSv8.3.0 and use the built in XDS510USB Debug Probe. It is still pretty current and thoroughly supports the C67x family of devices.

    - Update to CCSv9.0.0 and purchase TMDSEMU560V2STM-U Debug Probes. It will support CCSv9 and other architectures (such as the LCDK OMAPL138 mentioned in your other discussion). However, it is an expensive alternative.

    I will try to contact other folks and see if they can propose alternatives. 

    Regards,

    Rafael


    I recently moved to the Bluetooth Low Energy group and I am not active on the Code Composer Studio forum anymore.


    If my reply answers your question please click on the green button "This resolved my issue".

    Useful pages: Find bugs: New system (SIR), Old system (SDOWP), www.ti.com/jtag, Projects and Build, Debug, Download CCS

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.