This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2650: CC2650

Part Number: CC2650
Other Parts Discussed in Thread: CC2541,

Tool/software: Code Composer Studio

Dear E2E,
I am in the process of migrating from the reference design of the cc2541 to cc2650. This thread marked RESOLVED seems to indicate that this matter has been resolved. I have investigated the thread [Resolved] Migrating CC2541 to CC2650, which are the APIs for hal_delay_ms() and ll_McuPrecisionCount() - Bluetooth® forum - Bluetooth® - TI E2E Community
but this thread seems to point at a matter that is much further along and much deeper  in the transition which is beyond the starting point of the novice that I am and querying about. The resolved thread appears to have assumed such premise. I need to see which IDE I should begin to work with as I transition from the reference design of the cc2541 which IAR based IDE  to the cc2650 launchpad which is CCS compatible. Can I import the cc2541 reference design folder to the CCS and revise it to run it on the cc2650 or is there something that I need to do to the reference design within IAR environment to export it so it may be read by the CCS which is the design environment used by the 2650. Thank you for your patience. 
thanks