Part Number: MSP-TS430PN80USB
Tool/software: Code Composer Studio
Hello,
I am trying to test computationally intensive code my MSP430 platform that requires me to increase the size of the stack from the default value. However, when I change this value it does not seem to effect the maximum stack size displayed when I look at the "Stack Usage" tool within View->Stack Usage (screen shot attached with stack size changed to 4800.) The max stack size value seems to be pegged at 660 no matter what I set the maximum value to be in the settings. Interestingly, the "Memory Allocation" does seem to change as a function of the max stack size value I set (screen shot also attached.)
I am changing the stack size by editing the "Set C system stack size" field within Project->Properties.->CCS Build->MSP430 Linker->Basic options to 4800. Also, when I check my "..._linkInfo.xml" file the "__STACK_SIZE" field is updating to the value I set.
Compiler version: TI v18.1.5.LTS
Please let me know if any additional information would be helpful here.