Tool/software: Code Composer Studio
Respected,
SRR demo is suggested by one of the expert in TI for better performance . Please refer the below link to get some idea that i am talking about.
https://e2e.ti.com/support/sensors/f/1023/t/827835
And i started using AWR1642boost by flashing with SRR SDK code. But when i am using SRR visualizer to see the outputs of AWR i am getting some static objects reflections which is undesired in my application .To remove the static reflections i did not find any static clutter removal option in SRR visualizer . Why i am concerned of the static objects is the reflections from the static clutter is very strong when compared with humans reflection and the strong reflects will suppresses the weak signals to detected (which is resultant of 40 m above reflection of human).
Q1: How can i remove static clutter in SRR visualizer. Is there any possibility?
Q2: unlike mmwave demo the SRR output is not cluster data , but i need cluster what can i do to get the cluster data.
Please answer to my questions as fast as possible. Thanks in advance .