Tool/software: Code Composer Studio
I am trying to connect to Spectrum Digital eZdsp for TMS320F2808.
I am using Code Composer 9.1. on Windows 10.
I contacted SD and was told that this device contains an internal jtag and all I need to do is connect directly to the USB on my laptop.
When configuring the Device on the General Project tab I selected the Variant (280x Fixed Point and TMS320F2808).
The Connection: list only contains choices for XDS560V2 STM USB Emulator or XDSPro Emulator. When I press the Verify using either
of those choices I receive "E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_OPEN::dtc_conf"
I have also tried un-checking the "Manage the project's target-configuraiton automatically"
I checked the Windows device manager and I can see the "SD USB Based Debug Tools - Spectrum Digital eZdsp28xx USB" listed so I believe the drivers are installed correctly.
Is there any info on how to correctly configure for use with this device.
Thanks.