Part Number: MSP-EXP432P401R
Tool/software: Code Composer Studio
Using CCS + TExaSdisplay (someone knows why the upper/lower case is as it is? ) as per instructed in sekp066.pdf page 10 to 12, my TExaSdisplay display is dead.
The program is running fine, the LEDs are flashing (OK, I changed the delays so they become perceptible by a human being), so the problem is not there.
I got confirmation by TExaSdisplay that it found COM5 in my case, and it is the same USB cable that the one I got with the robot kit, so the cable and the communication should not be the problem.
But I don't get any clock signal (even with the event trigger set on raising edge for P1.0.
Any idea? I even close CCS, just in case the debugger could interfere. No candy.
By the way, (another question, but highly connected) the sekp066.pdf mentions that we could use our own Logic Analyzer if we have one. Nice, thanks you to give the permission, :-) , but where would I pin, say on a scope, the probe to get P1.0 clock signal? I don't see any pin with a remotely similar label on the development board.
Software versions:
CSS 9.2.0.00013 (the one with a red cube logo),
TExaSdisplay 2.4,
Windows 10 64 bits build 18362.418,
HP Desktop computer.