Part Number: TMS320F28335
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hi,
I want to run my BLDC motor with the help of my DSP(TMS320F28335). However it is able to detect change in Hall State ( I confirmed it by rotating rotor with hand). But as soon as Hall State is changing, corresponding pulses is not developed. However after when I stop the debugging and debug it again then corresponding correct pulses are produced. I am not getting how to develop pulses continuously according to change in hall state. I am using following code-
#define H_A GpiodataRegs.GPADAT.bit.GPIO24
#define H_ B GpiodataRegs.GPADAT.bit.GPIO25
#define H_C GpiodataRegs.GPADAT.bit.GPIO26
if (H_A == 1)
H1=1;
else H1=0;
if (H_2 == 1)
H2=1;
else H2=0;
if (H_C == 1)
H3=1;
else H3=0;
then calculating corresponding hall state and the switching.