Tool/software: Code Composer Studio
Hi,
I recently upgraded to CCS9.2.0.00013, installed on windows 7 x64. I can’t use the debugger, since the application always closes unexpectedly when I try to watch variables in the “Expressions” window, or when I switch to “Variables” window.
I’m using XDS200 connected to a TMS320C6678 and I would like to debug my code ported to CCS9, but it is actually impossible with this issue.
I already reported the error through the automatic procedure which activates when restarting CCS after unexpected crashes. I would like to know if there might be any parameter setting that I could try to mitigate the problem, while waiting for a new CCS update that would solve the problem.
Also, it looks like incremental building is not preserved through CCS sessions. My project is always recompiled completely whenever CCS is restarted, even if no file was changed. After first compilation, within a CCS session, incremental building works fine instead. I haven’t experimented it with previous CCS versions. Should it be the correct behavior?
Kind Regards,
Alessandro