Part Number: CC1312R
Other Parts Discussed in Thread: TIDA-010024, CC1350
Tool/software: Code Composer Studio
Hello,
I am trying to debug the 6lowpan code on our custom board having CC1312R. When I debug the example code of UART echo the UART works fine. When I try to send a string from the 6lowpan example(TIDA-010024) the debugger crashes with unable to access DAP error. I think it maybe because the UART is being used for the debugger and the code. Is there any workaround for this? UART2 pins are unavailable in our schematic so I cannot use uart2 to transmit data.
Regards,
Sabin