Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
Hi Everybody,
Few day ago the installed CCS v9.3.0.00012 was reported that there is a new update available for MSP432 tool-chain (version 8.2.3). I've intalled it without any problem.
After a restart of the CCS i'm not able to debug the MSP432P401M in our design. I'm using MSP-FET and XDS110 USB Debug Probe. The following error message appears:
CORTEX_M4_0: GEL: Error loading file 'C:\ti\ccs930\ccs\ccs_base\emulation\gel\msp432p401m.gel': line 327: expecting EOF, found '}'
and also:
CORTEX_M4_0: Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x14f98: (Error -614 @ 0x14F98) The target indicates there is an error condition from a previous SWD request. Clear the error the condition, and try the SWD request again. (Emulation package 8.4.0.00006)
CORTEX_M4_0: Breakpoint Manager: Retrying with a AET breakpoint
CORTEX_M4_0: Breakpoint Manager: _JobHardwareBreakpoint::ARM_DEBUG_V7M_fpb_add_breakpoint: Register/memory read failure[22004]
CORTEX_M4_0: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x6fac: (Error -615 @ 0x6FAC) The target failed to see a correctly formatted SWD header. The connection to the target may be unreliable. Try lowering the TCLK setting before trying again. (Emulation package 8.4.0.00006)
CORTEX_M4_0: Trouble Removing Breakpoint with the Action "Finish Auto Run" at 0x6fac: (Error -2044 @ 0x6FAC) Internal error: Requested breakpoint does not exist. Restart the application. If error persists, please report the error. (Emulation package 8.4.0.00006)
CORTEX_M4_0: JTAG Communication Error: (Error -615 @ 0x0) The target failed to see a correctly formatted SWD header. The connection to the target may be unreliable. Try lowering the TCLK setting before trying again. (Emulation package 8.4.0.00006)
What is wrong? What can I do now?
Thanks,
Zoltan Lencses