Part Number: C6000-CGT
Tool/software: TI C/C++ Compiler
Given the code example:
#include <utility>
int main()
{
auto retPair = std::make_pair(-1, false);
return retPair.first;
}
compiled as follows:
$CGT_PATH/bin/cl6x -I$CGT_PATH/include example.cpp --issue_remarks -pdv -pden)
The compiler produces the following output:
"example.cpp", line 5: remark #342-D: value copied to temporary, reference to
temporary used
auto retPair = std::make_pair(-1, false);
^
"example.cpp", line 5: remark #342-D: value copied to temporary, reference to
temporary used
auto retPair = std::make_pair(-1, false);
^
Since this is the typical use-case of std::make_pair (and std::make_pair's signature is changed to accept rvalue references in C++14 which are created specifically to allow references to temporaries), I would not expect such a diagnostic.
Due to this bug, I have to suppress the 342 diagnostic. This is undesirable, since a correct 342 diagnostic would (in general) indicate a pretty serious and hard to debug problem.