Tool/software: Code Composer Studio
I just received a LP-CC2652RB and am having issues in Code Composer.
I'm running Windows 10 as a development platform.
I've download and installed the more recent version of Code Composer Studio - Version 10.1.0.00010
I've imported portable_CC26X2R1_LAUNCHXL_tirtos_gcc, which builds wih no issues.
When I try to start the debugger the last thing I see on in the console window is
Cortex_M4_0: GEL Output: Memory Map Initialization Complete.
Cortex_M4_0: GEL Output: Board Reset Complete.
The debug console shows
The red and green LED's are both illuminated.
At this point everything freezes and I have to close CCS.
At one point I got a message directing me to examine the device. The following is what I saw
C:\ti\ccs1010\ccs\ccs_base\common\uscif\xds110>xdsdfu -e
USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated. All rights reserved.
Scanning USB buses for supported XDS110 devices...
<<<< Device 0 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Embed with CMSIS-DAP
Version: 3.0.0.13
Manufacturer: Texas Instruments
Serial Num: L12000VB
Mode: Runtime
Configuration: Standard
Found 1 device.
Thanks for any input.