Part Number: TM4C129CNCPDT
Tool/software: Code Composer Studio
Hello.
I've used CCS6 to build and debug my project successfully until today, but after transferring it to CCS10, I've encountered a problem to debug it properly -
After pressings the 'debug' button and flashing the program to the CPU I'm using(CORTEX_M4_1), the console outputs the following error lines -
CORTEX_M4_1: Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0xecd4: (Error -1066 @ 0xECD4) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.2.0.00002)
CORTEX_M4_1: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0xe752: (Error -1066 @ 0xE752) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.2.0.00002)
CORTEX_M4_1: Trouble Removing Breakpoint with the Action "Finish Auto Run" at 0xe752: (Error -2044 @ 0xE752) Internal error: Requested breakpoint does not exist. Restart the application. If error persists, please report the error. (Emulation package 9.2.0.00002)
I've already tried to search those errors online and follow suggested solutions, but it still haven't solved my problem.
Thanks for helpers.
Have a nice day.