Hello, I had format my PC and download latest version of CCS v8 and added my project for OMAPL138 DSP Core. this is using SDK v6.46.5.55, IPC v3.46.0.02, UIA v2.0.6.52 and XDC v3.32.2.25 and the Compiler version was 8.2.2
In the CCS v8, currently I am using the following :
SDK v6.46.5.55, IPC v3.50.4.08, UIA v2.30.1.02 and XDC v3.32.2.25 and the Compiler version was 8.3.2
But getting the following error:
>> Compilation failure
subdir_rules.mk:19: recipe for target 'build-823601265-inproc' failed
"package/cfg/app_pe674.c", line 2270: warning: a value of type "xdc_Ptr (*)(xdc_CPtr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)" cannot be used to initialize an entity of type "xdc_Ptr (*)(xdc_Ptr, xdc_SizeT, xdc_Ptr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)"
"package/cfg/app_pe674.c", line 2292: warning: a value of type "xdc_Ptr (*)(xdc_CPtr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)" cannot be used to initialize an entity of type "xdc_Ptr (*)(xdc_Ptr, xdc_SizeT, xdc_Ptr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)"
"package/cfg/app_pe674.c", line 2383: warning: a value of type "xdc_Ptr (*)(xdc_CPtr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)" cannot be used to initialize an entity of type "xdc_Ptr (*)(xdc_Ptr, xdc_SizeT, xdc_Ptr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)"
"package/cfg/app_pe674.c", line 2406: warning: a value of type "xdc_Ptr (*)(xdc_CPtr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)" cannot be used to initialize an entity of type "xdc_Ptr (*)(xdc_Ptr, xdc_SizeT, xdc_Ptr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)"
"package/cfg/app_pe674.c", line 2428: warning: a value of type "xdc_Ptr (*)(xdc_CPtr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)" cannot be used to initialize an entity of type "xdc_Ptr (*)(xdc_Ptr, xdc_SizeT, xdc_Ptr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)"
"package/cfg/app_pe674.c", line 2732: warning: a value of type "xdc_Ptr (*)(xdc_CPtr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)" cannot be used to initialize an entity of type "xdc_Ptr (*)(xdc_Ptr, xdc_SizeT, xdc_Ptr, const xdc_UChar *, xdc_SizeT, xdc_runtime_Error_Block *)"
"package/cfg/app_pe674.c", line 6950: error: identifier "CT__ti_ipc_family_omapl138_VirtQueue_Modul