Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650
Tool/software: Code Composer Studio
All attempts to use dev.ti.com and the TI Cloud to reprogram two working CC2650 Launchpad boards back to their factory applications fail with the message shown below:
I can confirm that the CC2650 Launchpad is indicating that firmware update has been kicked-off. The LED next to the XDS110 is flashing the typical alternating red/green pattern seen during flash programming. However, after reboot I see that the previous application is still in place. Cycling power and attempting download again always yields the same results.
I can also confirm that the data file is present in the temp folder, but it contains nothing but a single tag '[object Blob]'
Is this a known issue, and if so, what is the resolution?
If this can't be resolved can TI provide the hex file for this application so I can revert these boards manually with Flash Programmer 2?
Thanks.