Hi
we purchased a floating license for CCS5. Our server is a 32-bit CentOS 5.5, running as a virtual server under Dell OEM version of VMware ESXi (aka VMware vSphere) 4.1. Attempting to use install and use lmgrd, I get the following in the log:
21:50:59 (lmgrd) License file(s): /opt/license_server/licenses/TMDSCCS-ALLF01-v5.lic
21:50:59 (lmgrd) lmgrd tcp-port 27000
21:50:59 (lmgrd) Starting vendor daemons ...
21:50:59 (lmgrd) Using vendor daemon port 27100 specified in license file
21:50:59 (tidspssw) FLEXnet Licensing version v11.4.100.0 build 50818 i86_re3
21:50:59 (tidspssw) lmgrd version 11.10, tidspssw version 11.4
21:50:59 (lmgrd) Started tidspssw (internet tcp_port 27100 pid 5646)
21:50:59 (tidspssw) Server started on localhost for: CCS_CONNECTION_ALL
21:50:59 (tidspssw) CCS_DEBUGGER CCS_LINKER_FULL CCS_ISA_ALL
21:50:59 (tidspssw) EXTERNAL FILTERS are OFF
21:51:09 (tidspssw) Vendor daemon can't talk to lmgrd (Cannot connect to license server system. (-15,570:115 "Operation now in progress"))
21:51:09 (tidspssw) EXITING DUE TO SIGNAL 37 Exit reason 5
21:51:09 (lmgrd) tidspssw exited with status 37 (Communications error)
21:51:09 (lmgrd) Since this is an unknown status, license server
21:51:09 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
...
Hosts file contains:
127.0.0.1 localhost.localdomain localhost centos this_host
#::1 localhost6.localdomain6 localhost6
98.129.139.41 et1.sourcehosting.net et1
#192.168.101.41 this_host
License file contains
#Please Do not delete this comment line.
#SERVER this_host 000C298D865A
SERVER localhost 000C298D865A 27000
#SERVER 192.168.101.41 000C298D865A
VENDOR tidspssw PORT=27100
USE_SERVER
INCREMENT CCS_CONNECTION_ALL tidspssw 5.99 permanent 1 \
VENDOR_STRING=...
....
This problem did not show when install was attempted on an Ubuntu machine. However, I must use CentOS.
Help will be greatly appreciated.