Other Parts Discussed in Thread: OMAP-L138, OMAPL138
CCS tells me it "Cannot find a driver for PRU_0" and "Cannot find a driver for PRU_1".
(I just upgraded to CCS v5.4.0.00091, and this error is new to me. So, perhaps these clues are related?)
The CCS error report lists the resource as: LogicPD EVM OMAP-L138 -XDS100v2.ccxml . That configuration file uses two gel files: OMAPL138_ARM.gel and OMAPL138_DSP.gel. But it doesn't contain anything for the two PRUs.
(I'm trying to work with the ARM on the OMAP-L138. Yet it's flagging an error with the PRU_x.)
How do I solve this?
Thanks for your help.