Other Parts Discussed in Thread: CCSTUDIO
Hello,
When I link my C2000 project in CCS 3.3, the linker options (in the .lkf file) have the following include paths:
-i"C:/CCStudio_v3.3/C2000/xdais/lib"
-i"C:/CCStudio_v3.3/bios_5_31_02/packages/ti/bios/lib"
-i"C:/CCStudio_v3.3/bios_5_31_02/packages/ti/rtdx/lib/c2000"
-i"C:/Program Files/Texas Instruments/C2000 Code Generation Tools 5.2.0/lib"
None of these appear in the linker build options that I set for the project. The last one is probably fair enough, but the project does not use BIOS so why are the other libraries included?
More curiously: where in CCS is the option that controls that these paths are to be included in the linker options?
More importantly: is the inclusion of these libraries causing my resulting executable code to be larger than needed?
Cheers,
John.
Edit: LH: moving to CCS forum