Hello everyone
I just install new CCS6.1.1. However, when I import my previous ARM project from CCS 6.1.0 to CCS 6.1.1 project. It has errors. First, in the General Tab of project properties. It shows warning. You can see it in the attached picture. If I ignore this warning, the compiling would has error of that
This project was created using a version of compiler that is not currently installed: GNU_4.8.4:Linaro [ARM]. Please go to CCS App Center to install the compiler of this version, or migrate the project to one of the available compiler versions by adjusting project properties.
Build stopped..
In the Help->Installed Details, I can see GCC ARM compiler tools is installed (ver 4.8.0.2014q3). Even if I just copy the source file into newly create ARM project. it still has the same problem. Then I tried to install the "TI ARM compiler" in the CCS App Center, another error would be shown during the installation, said that :"
An error occurred while collecting items to be installed
session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Unable to read repository at http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/codegen/Updates/p2win32/binary/com.ti.cgt.tms470.5.2.win32_root_5.2.5.
Connection reset
.
Can anyone help me with that?
Thanks.
Xining