I purchased a ezdsp5535 board and have compiled and run the associated led_test program without any problem. I then try to get the CSL_USB_CdcExample_Out to run on this board and the program compiles giving no errors or warnings, but when the debugger tries to download to the board, a window pops up stating "Load program Error. Encountered a problem loading file: ..... .out Could not open file."
In checking the program's Debug directory, there are no .out, .map, or .obj files, while there are these files for the led_test program.
So my question is, why would there be no .out, .map, or .obj files when the compile and link give no errors or warnings and Code Composer tries to download the .out file to the target?
Any advise on what to check would greatly be appreciated! And yes, I didn't find anything helpful by searching the TI site.
Thank you,
Tom