Hello people!
The idea is I am very happy to see CCS coming to mac. The only concern I have now is that under Windows, my MSP432 launchpad is seen by the OS as a couple of virtual COM ports, so I just write some code, open any terminal and can "talk" to my launchpad, or debug through the COM terminal. That is great, because I can send some commands, print debug data and much more.
So is there an ability to do the same thing under Mac? So that I just could open terminal and talk to my launchpad? Perhaps there is some built-in COM port terminal in CCS? I don't know.. Just any advice would be greatly appreciated.