This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

macro concatenation with ++ does not create a valid token



Hello, I've been trying to implement this macro function. It is from professor Valvano. It works in Keil, but doesn't work on CCS. 

When I compile it, CCS shows:

Please, how do I configure CCS to run this code?

Thank you.

// create index implementation FIFO (see FIFO.h)
AddIndexFifo(Rx, FIFOSIZE, char, FIFOSUCCESS, FIFOFAIL)



// FIFO.h
// Runs on any LM3Sxxx
// Provide functions that initialize a FIFO, put data in, get data out,
// and return the current size. The file includes a transmit FIFO
// using index implementation and a receive FIFO using pointer
// implementation. Other index or pointer implementation FIFOs can be
// created using the macros supplied at the end of the file.
// Daniel Valvano
// June 16, 2011

/* This example accompanies the book
"Embedded Systems: Real Time Interfacing to Arm Cortex M Microcontrollers",
ISBN: 978-1463590154, Jonathan Valvano, copyright (c) 2015
Programs 3.7, 3.8., 3.9 and 3.10 in Section 3.7

Copyright 2015 by Jonathan W. Valvano, valvano@mail.utexas.edu
You may use, edit, run or distribute this file
as long as the above copyright notice remains
THIS SOFTWARE IS PROVIDED "AS IS". NO WARRANTIES, WHETHER EXPRESS, IMPLIED
OR STATUTORY, INCLUDING, BUT NOT LIMITED TO, IMPLIED WARRANTIES OF
MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE.
VALVANO SHALL NOT, IN ANY CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL,
OR CONSEQUENTIAL DAMAGES, FOR ANY REASON WHATSOEVER.
For more information about my classes, my research, and my books, see
users.ece.utexas.edu/.../
*/

#ifndef __FIFO_H__
#define __FIFO_H__

long StartCritical (void); // previous I bit, disable interrupts
void EndCritical(long sr); // restore I bit to previous value



// macro to create an index FIFO
#define AddIndexFifo(NAME,SIZE,TYPE,SUCCESS,FAIL) \
uint32_t volatile NAME ## PutI; \
uint32_t volatile NAME ## GetI; \
TYPE static NAME ## Fifo [SIZE]; \
void NAME ## Fifo_Init(void){ long sr; \
sr = StartCritical(); \
NAME ## PutI = NAME ## GetI = 0; \
EndCritical(sr); \
} \
int NAME ## Fifo_Put (TYPE data){ \
if(( NAME ## PutI - NAME ## GetI ) & ~(SIZE-1)){ \
return(FAIL); \
} \
NAME ## Fifo[ NAME ## PutI &(SIZE-1)] = data; \
NAME ## PutI ## ++; \
return(SUCCESS); \
} \
int NAME ## Fifo_Get (TYPE *datapt){ \
if( NAME ## PutI == NAME ## GetI ){ \
return(FAIL); \
} \
*datapt = NAME ## Fifo[ NAME ## GetI &(SIZE-1)]; \
NAME ## GetI ## ++; \
return(SUCCESS); \
} \
unsigned short NAME ## Fifo_Size (void){ \
return ((unsigned short)( NAME ## PutI - NAME ## GetI )); \
}
// e.g.,
// AddIndexFifo(Tx,32,unsigned char, 1,0)
// SIZE must be a power of two
// creates TxFifo_Init() TxFifo_Get() and TxFifo_Put()

// macro to create a pointer FIFO
#define AddPointerFifo(NAME,SIZE,TYPE,SUCCESS,FAIL) \
TYPE volatile *NAME ## PutPt; \
TYPE volatile *NAME ## GetPt; \
TYPE static NAME ## Fifo [SIZE]; \
void NAME ## Fifo_Init(void){ long sr; \
sr = StartCritical(); \
NAME ## PutPt = NAME ## GetPt = &NAME ## Fifo[0]; \
EndCritical(sr); \
} \
int NAME ## Fifo_Put (TYPE data){ \
TYPE volatile *nextPutPt; \
nextPutPt = NAME ## PutPt + 1; \
if(nextPutPt == &NAME ## Fifo[SIZE]){ \
nextPutPt = &NAME ## Fifo[0]; \
} \
if(nextPutPt == NAME ## GetPt ){ \
return(FAIL); \
} \
else{ \
*( NAME ## PutPt ) = data; \
NAME ## PutPt = nextPutPt; \
return(SUCCESS); \
} \
} \
int NAME ## Fifo_Get (TYPE *datapt){ \
if( NAME ## PutPt == NAME ## GetPt ){ \
return(FAIL); \
} \
*datapt = *( NAME ## GetPt ## ++); \
if( NAME ## GetPt == &NAME ## Fifo[SIZE]){ \
NAME ## GetPt = &NAME ## Fifo[0]; \
} \
return(SUCCESS); \
} \
unsigned short NAME ## Fifo_Size (void){\
if( NAME ## PutPt < NAME ## GetPt ){ \
return ((unsigned short)( NAME ## PutPt - NAME ## GetPt + (SIZE*sizeof(TYPE)))/sizeof(TYPE)); \
} \
return ((unsigned short)( NAME ## PutPt - NAME ## GetPt )/sizeof(TYPE)); \
}
// e.g.,
// AddPointerFifo(Rx,32,unsigned char, 1,0)
// SIZE can be any size
// creates RxFifo_Init() RxFifo_Get() and RxFifo_Put()

#endif // __FIFO_H__

unsigned short NAME ## Fifo_Size (void){ \
return ((unsigned short)( NAME ## PutI - NAME ## GetI )); \
}