I created the following target configuration:
Connection is Texas Instruments XDS100v2 USB Debug Probe,
Board is EVM5517
The 5517 EVM is assy 514660 rev F
When I try to connect to the target I get the following error:
I tried running the xds100serial utility and get the message: No XDS100 emulators were found on the system.
I'm running CCS 6.2 under Windows 7 Professional
The Windows Device Manager shows under SD USB Based Debug Tools ... 'Spectrum Digital TMS320C5510 DSK'
I also tried a different target configuration: Spectrum Digital DSP-EVM-eZdsp onboard USB Emulator, but using this one, I get an 'Error initializing emulator' message instead.
I've tried uninstalling this driver then reinstalling it, and changing USB ports on my machine. Nothing works. Any suggestions on how to get the emulator working would be greatly appreciated!
Thanks,
Jim