Dear Code Componser,
I am debugging an application for the C28375D.
In general all appears working, however I'm not sure how to interpret the following behavior.
I have setup CPU1 and CPU2, and CLA (on CPU2)
The CLA on CPU2 is reading the ADCs and interrupting CPU2 to deliver the data.
So far it appears as if everything is working, however:
When I run it at on clock rate, I see CPU1 (Running) CPU2 (Running) and CPU2_CLA1 (Running) at the top of code composer. If I change the timer (rate of clocking the CLAs) I suddenly see CPU1 & 2 running... but CPU2_CLA1 keeps showing a variety of 'does not contain frame information...'.
Now the interesting part is... the source code goes to a portion of the code, as if it had hit a breakpoint... but I do nothing and a short while later, it goes to a different point in the code with some forme of 'does not contain frame information' and so on... periodically showing the code, then delay.. then shows another point in the code, delay etc... it is cycling between the same 3 points in the code where it claims something doesn't conatin frame information.
Now the application appears to be running even though it says CPU2_CLA1 is suspended...
So this is the confusing part...
Could you elaborate what behavior I am seeing?
To my knowledge if it says that CPU2_CLA1 is suspended it shouldn't be jumping anywhere... cause it's suspended... the fact it is says something odd I s happening, correct?