This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/OMAP3530: FUNC_ALWAYS_INLINE not inlining

Part Number: OMAP3530


Tool/software: TI C/C++ Compiler

I am getting error #18 expected a ")", with the following C code in a header file.

#pragma FUNC_ALWAYS_INLINE(func_svc0)

static inline void func_svc0(unsigned int x)
{
args[0] = x;

__asm(" push {lr} ");
__asm(" mov r1,pargs");
__asm(" svc #0");
__asm(" pop {lr} ");
}

#18 expected a ")"  for the above.  If I remove the func name from the pragma line I get a warning:

#830-D error processing pragma FUNC_ALWAYS_INLINE, verify format .

Compiler TI v5.2.7 for ARM, -O0