This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Zooming in Image Analyzer?

Hello,

 

In Image Analyzer of CCS 4, is there any way to zoom in/out an image? I looked through all possible options (View Menu, Image Analyzer context menu) but still cannot find one.

I remember in CCS 3.3 one could easily zoom/in out a displayed image. Is this function removed in version 4?

 

 

Jim

  • Jim,

    Once the image is displayed, you can control Zoom using the two magnifying glass icons at the top right of the Image window.

    Hope this helps,

    Rafael

  • Dear Rafael,

    It was so careless of me for failing to notice that. Thanks very much.

     

    Jim

  • Hi.Jim

    I'm new to CCS4. I have an application which deals with images. For debugging purpose I need to display them but it displays incorrectly. Probably I have the wrong Image Analyzer settings. Could you help me out?

     

    my Image Analyzer settings are

    Image format: RGB

     Num pixels per line: 80

     Data format: Packed

    Pixel stride: 1

     Red mask: 0xFFFFFFFF

     Green mask: 0xFFFFFFFF

    Blue mask: 0xFFFFFFFF

    Alpha mask: 0x0000

    Line stride: 1

     Image source: File

     Filename:D:\CCS4\WGCH\workspace\Histogram\1.bmp

     Read data as: 8-bit data

    Thanks

    GuoCHeng

  • Hi,

    I'm new to CCS4. I have an application which deals with images. For debugging purpose I need to display them but it displays incorrectly. Probably I have the wrong Image Analyzer settings. Could you help me out?

    my Image Analyzer settings are

    Image format: RGB

    Num pixels per line: 80

    Data format: Packed

    Pixel stride: 1

    Red mask: 0xFFFFFFFF

    Green mask: 0xFFFFFFFF

    Blue mask: 0xFFFFFFFF

    Alpha mask: 0x0000

    Line stride: 1

    Image source: File

    Filename:D:\CCS4\WGCH\workspace\Histogram\1.bmp

    Read data as: 8-bit data

    Thanks

    GuoCHeng