This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS: Memory_getStats exception

Tool/software: TI-RTOS

Dear Support Team,

When I call this method: 

    Memory_Stats stats;
    HeapMem_getStats(NULL, &stats);

I got the following error:

ti.sysbios.family.arm.m3.Hwi: line 1095: E_hardFault: FORCED
ti.sysbios.family.arm.m3.Hwi: line 1172: E_busFault: PRECISERR: Immediate Bus Fault, exact addr known, address: 140f04f4
Exception occurred in background thread at PC = 0x000b5530.
Core 0: Exception occurred in ThreadType_Task.
Task name: ConfigBoot, handle: 0x200035b8.
Task stack base: 0x20003620.
Task stack size: 0x800.
R0 = 0x09f3efbf  R8  = 0x00000001
R1 = 0x00000000  R9  = 0x00000000
R2 = 0x09f3efbf  R10 = 0xffffffff
R3 = 0x09f3efbf  R11 = 0xffffffff
R4 = 0x20003c78  R12 = 0x00000000
R5 = 0x20033fb8  SP(R13) = 0x20003c60
R6 = 0x00000000  LR(R14) = 0x000b866d
R7 = 0x140f04f0  PC(R15) = 0x000b5530
PSR = 0x21000000
ICSR = 0x00423803
MMFSR = 0x00
BFSR = 0x82
UFSR = 0x0000
HFSR = 0x40000000
DFSR = 0x00000000
MMAR = 0x140f04f4
BFAR = 0x140f04f4
AFSR = 0x00000000
Terminating execution...

I got the following headers included:

// to print heapSize
#include <xdc/runtime/Memory.h>
#include <ti/sysbios/heaps/HeapMem.h>

When I step inside the getStats() i can debug step by step, but later the exception fired.

I tried in different tasks not just ConfigBoot but same result. 

Can you help me how to go on?

Should I set anything in *.cfg? Is there any detailed description? Thank you in advance!