This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28069: Not possible to graph an array

Part Number: TMS320F28069

Tool/software: Code Composer Studio

Hi, 

I am working with Code Composer version: 7.4.0.00015.

I get an analog signal (sinusoidal waveform) via A/D converter and store it on an array of 300 position, defined as double MY_BUF[BUFFER_SIZE], where BUFFER_SIZE is 300.

My issue comes when trying to plot the array in a graph, I get an error message saying double[300] is 16. Only unsigned type of 32/64 bits supported.

I had never experienced this issue before, and I don't get any problems if I just put in graphs the same type of variable of only one position. 

Best regards,

Cristina