This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C5535: CCS v8 Python Scripting with DSS

Genius 13655 points
Part Number: TMS320C5535


Tool/software: Code Composer Studio

Hello Champs,

Customer wanted to use Python Scripting with DSS in CCS v8, but there is no dvt_scripting.jar in CCS v8. Can he use the dvt_scripting.jar in CCS v5 instead?



Thanks.
Rgds
Shine

  • Hello,

    Shine said:
    Customer wanted to use Python Scripting with DSS in CCS v8, but there is no dvt_scripting.jar in CCS v8. Can he use the dvt_scripting.jar in CCS v5 instead?

    It looks like dvt_scripting.jar was removed starting with CCSv8 (I see it in CCSv7). They probably could take it from CCSv7... but in any case it is likely not needed since the vast majority of DSS functionality is the other jar files which do exist (and I believe the DVT scripting stuff is being deprecated in support anyway).

    Thanks

    ki