Ever since I did a recent minor upgrade of CC I see annoying behavior with building/debugging. In Debug mode, when I do a build, it now takes the liberty of running debug. This takes over 40 seconds for just 1K bytes of obj code so I'd like to avoid doing debug runs when I just need to do a basic compilation. I couldn't find a CC or compiler switch to prevent this.
A related issue is that I can't deduce from the help doc exactly what the following functions are supposed to do:
* Build Active Project
* Rebuild Active Project
* Build All
* Build Automatically
* Debug active proj
* Launch TI Debugger
* Debug...
* Debug Launch (button)
Could somebody please clue me in or point me to doc which clearly explains the differences? It seems that build All builds everything in my workspace, including non-active projects? Thx.