Tool/software: TI C/C++ Compiler
Dear Sirs:
Based on the informations in below link:
The C6000 CGT v8.3.x should support C++14.
However the std::atomic which is supported from c++11 is not supported in the above 8.3.x tools.
My question is that does C6000 CGT v8.3.x support full C++14 or it only support part of the C++14 inside it?
Where can I know what features in C++14 are supported in TI CGT C6000 v8.3.x?
Regards,
/ckhsu