This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

examples projects

hi,

i've just installed the CCS 4 and i tried to load an example project.

a related path is given in the "welcome" window, however i can not find it.

where can i find these example files?

thanks.

 

  • Hi,

    A nice starting guide that helps becoming familiar with CCSv4 is at the page below:

    http://processors.wiki.ti.com/index.php/CCSv4_Getting_Started_Guide

    Pay special attention to the section Working with CCS that contains a step-by-step guide on how to create and debug an example project with CCS.

    Depending on the device family you are using, you may find other example projects in the

    Hope this helps,

    Rafael

  •  

    Which ISA or "Device" examples are you looking for. MSP430? If so, you can find some included examples under the directory "\ccsv4\MSP430\examples". For example, if you used the default install options, that would be  "C:\Program Files\Texas Instruments\ccsv4\msp430\examples".

    Raj