Tool/software: TI C/C++ Compiler
Every time I compile my project I get lots of useless remarks like these (which I'm ignoring, but I'd prefer a clean compile):
"/Applications/ti/ccs1010/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/include/new.stdh", line 135: remark #885-D: support for placement delete is disabled "/Applications/ti/ccs1010/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/include/stlport/s__cstddef.h", line 26: remark #195-D: zero used for undefined preprocessing identifier "__GNUC__" "/Applications/ti/ccs1010/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/include/math.h", line 113: remark #195-D: zero used for undefined preprocessing identifier "__STDC_VERSION__"
These seem to only occur when these headers are included from C++ source files.
All of these should be easy to fix by editing the header files.
I see that someone reported this here back in 2011 for the CGT version 5.2 and it's still an issue in the latest compiler.