Other Parts Discussed in Thread: SEGGER,
Tool/software: Code Composer Studio
Hello all,
I have troubles to use the segger j-Link. with the cJTAG configuration.
I get the following error:
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: Error: Stat [ JLINKARM_IsHalted() call ] failed!
Cortex_M3_0: Unable to determine target status after 20 attempts
The hardware should be ok, If I use the xds110 from the launchpads it works, and if i check the connection with the segger tool it is ok (see below). But if I use the CCS I do not get a connection.
BR Noge