Tool/software: TI C/C++ Compiler
Hi Karan,
I have gone through query https://e2e.ti.com/support/processors/f/791/p/903161/3351424?tisearch=e2e-quicksearch&keymatch=ipc_echo_testb#pi320966filter=all&pi320966scroll=false
We are also facing the similar issue.
We have binary application.out from 3rd party vendor. We want to boot application.out from SD Card (Using SBL). To boot the binary using SBL, We have kept reset vector to BTCM (In the linker file), still it's not working as expected.
Working scenario : Keep binary [SBL(tiboot3.bin), sysfw.bin, app(provided by TI)] in SDCard then load application.out from CCS.
Not working scenario: Instead of app provided by TI, we are keeping 3rd party application.out (rename as app).
I don't have source code and linker file of app which is provided by TI. But I understood from mcusw demos like we have to keep reset vector to BTCM. I have tried those changes but not working.
Once it work with SBL then we want to boot application.out from SPL with Linux running on A72.
It will be good if you can help here.
Thanks,
-Makani