Dear TI:
I have a urgency problem, My board deserializer is DS90UB960, serializer is DS90UB935, Sensor is AR0234, 1920*1080, FPS is 30fps, the SOC just have one camera(have one DS90UB953);
I want to generate a frame synchronization signal (FrameSync), so it can make camera generate picture, I see your DS90UB960 datasheet about FrameSync Operation, So I configure the register about 960 and 953, But I found that my configure failed.
then I print the register about deserializer and serializer, and I add my configure of deserializer and serializer, so can TI help me solve this problem?
#deserializer 960 configure, 0x30 represent deserializer 960
i2cset -y 3 0x30 0x01 0x01
i2cset -y 3 0x30 0x02 0x3e
i2cset -y 3 0x30 0x0c 0xab
i2cset -y 3 0x30 0x4c 0x01
i2cset -y 3 0x30 0x58 0x5e
i2cset -y 3 0x30 0x5c 0x84
i2cset -y 3 0x30 0x5d 0x84
i2cset -y 3 0x30 0x65 0x84
i2cset -y 3 0x30 0x6d 0x7c
i2cset -y 3 0x30 0x70 0x1e
i2cset -y 3 0x30 0x32 0x01
i2cset -y 3 0x30 0x21 0x83
i2cset -y 3 0x30 0x33 0x23
i2cset -y 3 0x30 0x1f 0x02
i2cset -y 3 0x30 0xb9 0x1f
# deserializer 960 frame sync
i2cset -y 3 0x30 0x4c 0x01
i2cset -y 3 0x30 0x6e 0x8a
i2cset -y 3 0x30 0x10 0x91
i2cset -y 3 0x30 0x58 0x5e
i2cset -y 3 0x30 0x19 0x15
i2cset -y 3 0x30 0x1a 0xb3
i2cset -y 3 0x30 0x1b 0xc3
i2cset -y 3 0x30 0x1c 0x50
i2cset -y 3 0x30 0x18 0x01
#serializer 953 configure, 0x42 represent serializer 953
i2cset -y 3 0x42 0x02 0x13
i2cset -y 3 0x42 0x0E 0x10
i2cset -y 3 0x42 0x0D 0x10