I am configuring the receive mailbox, as below:
- Message-ID: 0x00000003
- Message-ID mask: 0x00000007
- Message type: Extended
For F2837xD, the register window shows the proper value for the CAN_IF2MSK register. Please refer to the below screenshot.
But the F2838x, the register window does not show the proper value for the CAN_IF2MSK register. Please refer to the below screenshot.
The attached image for F2838x and F2837xD is from CCS 10.1.
I have checked the register values using CCS 10.2 as well after suggested in the post. But the values for the F2838x CAN_IF2Msk register are still the same as shown in the image.
Can you please check and let me know about this behavior?
Thanks,
Dhanashree