I'm having the following error message:
CORTEX_M4_0: GEL: Encountered a problem loading file: /Users/paolalondono/Desktop/lab3/Debug/lab3.out Could not open file
The code I wrote does not show any syntax error. It shows that the error comes from the library. I deleted the library, dowloaded a new copy of it and added it to my program several times to see if that will fix it. When I ran the build system, I checked for errors in the particular files that build shows, but I cannot find anything wrong with them. So at this point I don't know what else I should do.
This is my code:
/* Include header files */
#include "driverlib.h"
#include "mechrev.h"
/* Define macros and function prototypes if needed */
#define LED1 GPIO_PORT_P1,GPIO_PIN0
#define LEDR GPIO_PORT_P2,GPIO_PIN0
#define LEDG GPIO_PORT_P2,GPIO_PIN1
#define LEDB GPIO_PORT_P2,GPIO_PIN2
#define BTN1 GPIO_PORT_P1,GPIO_PIN1
#define BTN2 GPIO_PORT_P1,GPIO_PIN4
#define BMP0 GPIO_PORT_P4,GPIO_PIN0
#define BMP1 GPIO_PORT_P4,GPIO_PIN2
#define BMP2 GPIO_PORT_P4,GPIO_PIN3
#define BMP3 GPIO_PORT_P4,GPIO_PIN5
#define BMP4 GPIO_PORT_P4,GPIO_PIN6
#define BMP5 GPIO_PORT_P4,GPIO_PIN7
/* Declare global and volatile variables if needed */
/* Main program */
void main(void)
{
/* Stop Watchdog Timer */
MAP_WDT_A_holdTimer();
/* Call the mechrev_setup function included in the mechrev.h header file */
mechrev_setup();
/* Initialize GPIOs P1.1 and P1.4 for PushButtons (S1 and S2 switches) */
MAP_GPIO_setAsInputPinWithPullUpResistor(BTN1);
MAP_GPIO_setAsInputPinWithPullUpResistor(BTN2);
/* Initialize GPIOs P1.0, P2.0, P2.1 and P2.2 for LED1 and LED2 */
MAP_GPIO_setAsOutputPin(LED1);
MAP_GPIO_setAsOutputPin(LEDR);
MAP_GPIO_setAsOutputPin(LEDG);
MAP_GPIO_setAsOutputPin(LEDB);
MAP_GPIO_setOutputLowOnPin(LED1);
MAP_GPIO_setOutputLowOnPin(LEDR);
MAP_GPIO_setOutputLowOnPin(LEDG);
MAP_GPIO_setOutputLowOnPin(LEDB);
/* Initialize GPIOs P4.0, P4.2, P4.3, P4.5, P4.6 and P4.7 for Bump Sensors */
MAP_GPIO_setAsInputPinWithPullUpResistor(BMP0);
MAP_GPIO_setAsInputPinWithPullUpResistor(BMP1);
MAP_GPIO_setAsInputPinWithPullUpResistor(BMP2);
MAP_GPIO_setAsInputPinWithPullUpResistor(BMP3);
MAP_GPIO_setAsInputPinWithPullUpResistor(BMP4);
MAP_GPIO_setAsInputPinWithPullUpResistor(BMP5);
/* Enable interrupts for Bump Sensors' GPIOs */
MAP_GPIO_enableInterrupt(BMP0);
MAP_GPIO_enableInterrupt(BMP1);
MAP_GPIO_enableInterrupt(BMP2);
MAP_GPIO_enableInterrupt(BMP3);
MAP_GPIO_enableInterrupt(BMP4);
MAP_GPIO_enableInterrupt(BMP5);
MAP_GPIO_interruptEdgeSelect(BMP0,GPIO_HIGH_TO_LOW_TRANSITION);
MAP_GPIO_interruptEdgeSelect(BMP1,GPIO_HIGH_TO_LOW_TRANSITION);
MAP_GPIO_interruptEdgeSelect(BMP2,GPIO_HIGH_TO_LOW_TRANSITION);
MAP_GPIO_interruptEdgeSelect(BMP3,GPIO_HIGH_TO_LOW_TRANSITION);
MAP_GPIO_interruptEdgeSelect(BMP4,GPIO_HIGH_TO_LOW_TRANSITION);
MAP_GPIO_interruptEdgeSelect(BMP5,GPIO_HIGH_TO_LOW_TRANSITION);
Interrupt_enableInterrupt(INT_PORT4);
/* Declare local variables if needed */
/* Call the initialization grading macro */
MACRO_LAB3_INIT();
while(1)
{
/* Design a Polling process to detect PushButtons press and turn on or off LED1 accordingly */
if (MAP_GPIO_getInputPinValue(BTN1) == GPIO_INPUT_PIN_LOW || MAP_GPIO_getInputPinValue(BTN2) == GPIO_INPUT_PIN_LOW)
{
MAP_GPIO_setOutputHighOnPin(LED1);
}
else
{
MAP_GPIO_setOutputLowOnPin(LED1);
}
/* Note: Call the event grading macro after turning on LED1 */
MACRO_LAB3_EVENT();
}
}
/* Interrupt Service Routine for PORT4 to handle Bump Sensors */
void PORT4_IRQHandler(void)
{
/* Check the interrupt status */
uint32_t status;
status = MAP_GPIO_getEnabledInterruptStatus(GPIO_PORT_P4);
/* verify that the interrupt is triggered by P4.0 or P4.7 */
if (status & GPIO_PIN0 != 0 || status & GPIO_PIN7 != 0)
{
/* Change the color of LED2 to RED */
GPIO_setOutputHighOnPin(GPIO_PORT_P2,GPIO_PIN0); // red on
GPIO_setOutputLowOnPin(GPIO_PORT_P2,GPIO_PIN1); // green off
GPIO_setOutputLowOnPin(GPIO_PORT_P2,GPIO_PIN2); // blue off
// call the grading macro here when generating the grading outputs:
MACRO_LAB3_EVENT(); //
}
/* verify that the interrupt is triggered by P4.2 or P4.6 */
else if (status & GPIO_PIN2 != 0|| status & GPIO_PIN6 != 0)
{
/* Change the color of LED2 to GREEN */
GPIO_setOutputLowOnPin(GPIO_PORT_P2,GPIO_PIN0); // red off
GPIO_setOutputHighOnPin(GPIO_PORT_P2,GPIO_PIN1); // green on
GPIO_setOutputLowOnPin(GPIO_PORT_P2,GPIO_PIN2); // blue off
// call the grading macro here when generating the grading outputs:
MACRO_LAB3_EVENT();
}
/* verify that the interrupt is triggered by P4.3 or P4.5 */
else if (status & GPIO_PIN3 != 0|| status & GPIO_PIN5 != 0)
{
/* Change the color of LED2 to BLUE */
GPIO_setOutputLowOnPin(GPIO_PORT_P2,GPIO_PIN0); // red off
GPIO_setOutputLowOnPin(GPIO_PORT_P2,GPIO_PIN1); // green off
GPIO_setOutputHighOnPin(GPIO_PORT_P2,GPIO_PIN2); // blue on
// call the grading macro here when generating the grading outputs:
MACRO_LAB3_EVENT();
}
/* Clear the PORT4 interrupt flag */
MAP_GPIO_clearInterruptFlag(GPIO_PORT_P4, status);
}
****************************************************************************************************
When I run "Build" this is what I get:
**** Build of configuration Debug for project lab3 ****
/Applications/ti/ccs1000/ccs/utils/bin/gmake -k -j 7 all -O
Building file: "../MSP432P4xx/aes256.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/aes256.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/aes256.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/aes256.obj' failed
"../MSP432P4xx/aes256.c", line 37: fatal error #1965: cannot open source file "aes256.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/aes256.c".
Compilation terminated.
gmake: *** [MSP432P4xx/aes256.obj] Error 1
"../MSP432P4xx/comp_e.c", line 37: fatal error #1965: cannot open source file "comp_e.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/comp_e.c".
Compilation terminated.
gmake: *** [MSP432P4xx/comp_e.obj] Error 1
"../main.c", line 2: fatal error #1965: cannot open source file "driverlib.h"
1 catastrophic error detected in the compilation of "../main.c".
Compilation terminated.
gmake: *** [main.obj] Error 1
"../MSP432P4xx/adc14.c", line 42: fatal error #1965: cannot open source file "adc14.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/adc14.c".
Compilation terminated.
gmake: *** [MSP432P4xx/adc14.obj] Error 1
"../MSP432P4xx/cpu.c", line 37: fatal error #1965: cannot open source file "cpu.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/cpu.c".
Compilation terminated.
gmake: *** [MSP432P4xx/cpu.obj] Error 1
"../MSP432P4xx/cs.c", line 41: fatal error #1965: cannot open source file "cs.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/cs.c".
Compilation terminated.
gmake: *** [MSP432P4xx/cs.obj] Error 1
"../MSP432P4xx/dma.c", line 39: fatal error #1965: cannot open source file "debug.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/dma.c".
Compilation terminated.
gmake: *** [MSP432P4xx/dma.obj] Error 1
"../MSP432P4xx/flash.c", line 41: fatal error #1965: cannot open source file "flash.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/flash.c".
Compilation terminated.
gmake: *** [MSP432P4xx/flash.obj] Error 1
"../MSP432P4xx/fpu.c", line 37: fatal error #1965: cannot open source file "fpu.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/fpu.c".
Compilation terminated.
gmake: *** [MSP432P4xx/fpu.obj] Error 1
"../MSP432P4xx/i2c.c", line 37: fatal error #1965: cannot open source file "i2c.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/i2c.c".
Compilation terminated.
gmake: *** [MSP432P4xx/i2c.obj] Error 1
"../MSP432P4xx/gpio.c", line 41: fatal error #1965: cannot open source file "gpio.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/gpio.c".
Compilation terminated.
gmake: *** [MSP432P4xx/gpio.obj] Error 1
"../MSP432P4xx/mpu.c", line 37: fatal error #1965: cannot open source file "debug.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/mpu.c".
Compilation terminated.
gmake: *** [MSP432P4xx/mpu.obj] Error 1
"../MSP432P4xx/interrupt.c", line 41: fatal error #1965: cannot open source file "debug.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/interrupt.c".
Compilation terminated.
gmake: *** [MSP432P4xx/interrupt.obj] Error 1
"../MSP432P4xx/pmap.c", line 37: fatal error #1965: cannot open source file "debug.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/pmap.c".
Compilation terminated.
gmake: *** [MSP432P4xx/pmap.obj] Error 1
"../MSP432P4xx/pcm.c", line 41: fatal error #1965: cannot open source file "pcm.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/pcm.c".
Compilation terminated.
gmake: *** [MSP432P4xx/pcm.obj] Error 1
"../MSP432P4xx/reset.c", line 37: fatal error #1965: cannot open source file "reset.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/reset.c".
Compilation terminated.
gmake: *** [MSP432P4xx/reset.obj] Error 1
"../MSP432P4xx/ref_a.c", line 37: fatal error #1965: cannot open source file "ref_a.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/ref_a.c".
Compilation terminated.
gmake: *** [MSP432P4xx/ref_a.obj] Error 1
"../MSP432P4xx/pss.c", line 41: fatal error #1965: cannot open source file "pss.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/pss.c".
Compilation terminated.
gmake: *** [MSP432P4xx/pss.obj] Error 1
"../MSP432P4xx/rtc_c.c", line 37: fatal error #1965: cannot open source file "rtc_c.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/rtc_c.c".
Compilation terminated.
gmake: *** [MSP432P4xx/rtc_c.obj] Error 1
"../MSP432P4xx/spi.c", line 37: fatal error #1965: cannot open source file "spi.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/spi.c".
Compilation terminated.
gmake: *** [MSP432P4xx/spi.obj] Error 1
Building file: "../MSP432P4xx/comp_e.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/comp_e.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/comp_e.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/comp_e.obj' failed
"../MSP432P4xx/systick.c", line 37: fatal error #1965: cannot open source file "debug.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/systick.c".
Compilation terminated.
gmake: *** [MSP432P4xx/systick.obj] Error 1
"../MSP432P4xx/timer32.c", line 37: fatal error #1965: cannot open source file "timer32.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/timer32.c".
Compilation terminated.
gmake: *** [MSP432P4xx/timer32.obj] Error 1
"../MSP432P4xx/sysctl.c", line 42: fatal error #1965: cannot open source file "sysctl.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/sysctl.c".
Compilation terminated.
gmake: *** [MSP432P4xx/sysctl.obj] Error 1
"../MSP432P4xx/timer_a.c", line 37: fatal error #1965: cannot open source file "timer_a.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/timer_a.c".
Compilation terminated.
gmake: *** [MSP432P4xx/timer_a.obj] Error 1
"../MSP432P4xx/uart.c", line 37: fatal error #1965: cannot open source file "uart.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/uart.c".
Compilation terminated.
gmake: *** [MSP432P4xx/uart.obj] Error 1
"../MSP432P4xx/wdt_a.c", line 41: fatal error #1965: cannot open source file "wdt_a.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/wdt_a.c".
Compilation terminated.
gmake: *** [MSP432P4xx/wdt_a.obj] Error 1
Building file: "../main.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c"
>> Compilation failure
subdir_rules.mk:7: recipe for target 'main.obj' failed
Building file: "../MSP432P4xx/adc14.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/adc14.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/adc14.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/adc14.obj' failed
Building file: "../MSP432P4xx/cpu.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/cpu.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/cpu.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/cpu.obj' failed
Building file: "../MSP432P4xx/cs.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/cs.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/cs.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/cs.obj' failed
Building file: "../MSP432P4xx/dma.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/dma.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/dma.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/dma.obj' failed
Building file: "../MSP432P4xx/flash.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/flash.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/flash.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/flash.obj' failed
Building file: "../MSP432P4xx/fpu.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/fpu.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/fpu.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/fpu.obj' failed
"../MSP432P4xx/crc32.c", line 39: fatal error #1965: cannot open source file "debug.h"
1 catastrophic error detected in the compilation of "../MSP432P4xx/crc32.c".
Compilation terminated.
gmake: *** [MSP432P4xx/crc32.obj] Error 1
Building file: "../MSP432P4xx/i2c.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/i2c.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/i2c.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/i2c.obj' failed
Building file: "../MSP432P4xx/gpio.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/gpio.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/gpio.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/gpio.obj' failed
Building file: "../MSP432P4xx/mpu.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/mpu.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/mpu.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/mpu.obj' failed
Building file: "../MSP432P4xx/interrupt.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/interrupt.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/interrupt.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/interrupt.obj' failed
Building file: "../MSP432P4xx/pmap.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/pmap.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/pmap.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/pmap.obj' failed
Building file: "../MSP432P4xx/pcm.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/pcm.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/pcm.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/pcm.obj' failed
Building file: "../MSP432P4xx/reset.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/reset.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/reset.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/reset.obj' failed
Building file: "../MSP432P4xx/ref_a.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/ref_a.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/ref_a.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/ref_a.obj' failed
Building file: "../MSP432P4xx/pss.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/pss.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/pss.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/pss.obj' failed
Building file: "../MSP432P4xx/rtc_c.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/rtc_c.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/rtc_c.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/rtc_c.obj' failed
Building file: "../MSP432P4xx/spi.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/spi.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/spi.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/spi.obj' failed
Building file: "../MSP432P4xx/systick.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/systick.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/systick.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/systick.obj' failed
Building file: "../MSP432P4xx/timer32.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/timer32.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/timer32.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/timer32.obj' failed
Building file: "../MSP432P4xx/sysctl.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/sysctl.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/sysctl.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/sysctl.obj' failed
Building file: "../MSP432P4xx/timer_a.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/timer_a.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/timer_a.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/timer_a.obj' failed
Building file: "../MSP432P4xx/uart.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/uart.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/uart.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/uart.obj' failed
Building file: "../MSP432P4xx/wdt_a.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/wdt_a.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/wdt_a.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/wdt_a.obj' failed
Building file: "../MSP432P4xx/crc32.c"
Invoking: ARM Compiler
"/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include" --include_path="/Applications/ti/ccs1000/ccs/ccs_base/arm/include/CMSIS" --include_path="/Users/paolalondono/Desktop/lab3" --include_path="/Applications/ti/ccs1000/ccs/tools/compiler/ti-cgt-arm_20.2.0.LTS/include" --advice:power=all --define=__MSP432P401R__ --define=ccs -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="MSP432P4xx/crc32.d_raw" --obj_directory="MSP432P4xx" "../MSP432P4xx/crc32.c"
>> Compilation failure
MSP432P4xx/subdir_rules.mk:7: recipe for target 'MSP432P4xx/crc32.obj' failed
gmake: Target 'all' not remade because of errors.
**** Build Finished ****