This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS Hangs/Freeze when (apparently) moving from one location to another

I work from home and on site at different times of the week.  If I work at home on a project then go into work CCS freezes when I open it.  To remedy the situation I create a new workspace, The reload my project from Git.  Then when I take the computer home and open the new workspace same thing CCS freezes (repeat procedure).  Screen looks a little strange also, I have included a screen shot of CCS when it starts. The only way to get out of this situation is using the task manager to kill CCS.

So, my work around is to use Git to archive frequently and make a new workspace when I move from one location to another.

This happens every time without fail.

Code Composer Studio
Version: 10.2.0.00009

OS: Windows 10, v.10.0, x86_64 / win32
Java version: 1.8.0_144

I don't recall, but not sure, that this has happened previous to the 10.2 update.

The screen is filled as shown, but CCS only fills a small portion.  Note the Windows controls in the upper right corner.