Hi
So up til now I could install extensions (in this example the mmwave SDK) using
%CCS_EXE% -noSplash -data %QUM_DIR% -application com.ti.common.core.initialize -rtsc.productDiscoveryPath "%QUM_TI_DIR%\mmwave_sdk_03_05_00_04"
For our purposes we had to recompile some of the SDK libraries and hence have moved the SDK onto our own git repo. With the latest version of CCS the installation of such a product does not work anymore.
Even though the command ends successful
!ENTRY com.ti.common.core 1 0 2021-07-12 14:05:50.980 !MESSAGE path=ccs_base/DebugServer !ENTRY com.ti.common.core 1 0 2021-07-12 14:05:50.980 !MESSAGE debugServerDir=C:/ti/ccs1040/ccs/ccs_base/DebugServer Searching for deleted extension-sites to uninstall: Finished! Searching for new extension-sites to install: Finished!
In my project I get the message that "Product XXX is not currently installed and no compatible version is available. Please install this product or a compatible version.". Even if I add the path manually in CCS it does not recognize the product (the SDK in this case). This was working seamlessly in previous versions.
How can I now install/add changed products (such as an SDK, which evidently needs some modification sometimes)?