Hallo,
I'm trying to debug a program for a Sensorless BLDC motor control via the JTAGjet-CCS. I get already this Warning when I try load the program:
Warning:
Error 0x40001020/-1268
Warning during: Execution, Target,
Core is Locked up in Hard Fault or in NMI.
When I load the Program with boot_eth_out: I get on the console:
CORTEX_M3_0: AutoRun: Target not run as the symbol "main" is not defined
And with qs-bldc.out:
Warning:error 0x40001020/-1268 Warning during : Execution, Target, Core Is Locked up in Hard Fault or NMI
I need help to solve this problem