This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1350 launchpad: Error when building simple_peripheral_cc1350lp_stack_FlashROM

Other Parts Discussed in Thread: CC1350, CC2650

Hi everyone,

I'm new using TI CC1350 launchpad. I'm corrently trying to build the exemple simple_peripheral.

The first step is build simple_peripheral_cc1350lp_stack_FlashROM but I always have the fallowing error:

I have done a lot of research but I didnt found something work for me.

Do you have a notion what can be the problem and how can I solve it?

Thanks

>> Compilation failure
OSAL/subdir_rules.mk:9: recipe for target 'OSAL/osal.obj' failed
"C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal.c", line 381: error #167: too few arguments in function call
1 error detected in the compilation of "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal.c".
gmake[1]: *** [OSAL/osal.obj] Error 1
Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack/npi.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="NPI/npi.d_raw" --obj_directory="NPI" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack/npi.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack/npi.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx/mb_patch.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="HAL/Target/CC2650/_common/mb_patch.d_raw" --obj_directory="HAL/Target/CC2650/_common" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx/mb_patch.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx/mb_patch.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_bufmgr.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="OSAL/osal_bufmgr.d_raw" --obj_directory="OSAL" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_bufmgr.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_bufmgr.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_cbtimer.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="OSAL/osal_cbtimer.d_raw" --obj_directory="OSAL" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_cbtimer.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_cbtimer.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_clock.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="OSAL/osal_clock.d_raw" --obj_directory="OSAL" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_clock.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_clock.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_memory_icall.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="OSAL/osal_memory_icall.d_raw" --obj_directory="OSAL" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_memory_icall.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_memory_icall.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_pwrmgr.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="OSAL/osal_pwrmgr.d_raw" --obj_directory="OSAL" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_pwrmgr.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_pwrmgr.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/mcu/cc26xx/osal_snv_wrapper.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="OSAL/osal_snv_wrapper.d_raw" --obj_directory="OSAL" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/mcu/cc26xx/osal_snv_wrapper.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/mcu/cc26xx/osal_snv_wrapper.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_timers.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="OSAL/osal_timers.d_raw" --obj_directory="OSAL" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_timers.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/common/osal_timers.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles/gap.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="PROFILES/gap.d_raw" --obj_directory="PROFILES" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles/gap.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles/gap.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/stack/ble_dispatch.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="ICallBLE/ble_dispatch.d_raw" --obj_directory="ICallBLE" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/stack/ble_dispatch.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/stack/ble_dispatch.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/host/sm_ecc.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="PROFILES/sm_ecc.d_raw" --obj_directory="PROFILES" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/host/sm_ecc.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/host/sm_ecc.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/host/gattservapp_util.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="PROFILES/gattservapp_util.d_raw" --obj_directory="PROFILES" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/host/gattservapp_util.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/host/gattservapp_util.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/icall_startup.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="Startup/icall_startup.d_raw" --obj_directory="Startup" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/icall_startup.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/icall_startup.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/stack/ble_user_config.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="Startup/ble_user_config.d_raw" --obj_directory="Startup" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/stack/ble_user_config.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/stack/ble_user_config.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack/osal_icall_ble.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="Startup/osal_icall_ble.d_raw" --obj_directory="Startup" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack/osal_icall_ble.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack/osal_icall_ble.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/onboard.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="TOOLS/onboard.d_raw" --obj_directory="TOOLS" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/onboard.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/onboard.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles/gapbondmgr.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="PROFILES/gapbondmgr.d_raw" --obj_directory="PROFILES" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles/gapbondmgr.c"
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles/gapbondmgr.c"

Building file: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom/rom_jt.c"
Invoking: Arm Compiler
"C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/bin/armcl" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/config/build_components.opt" --cmd_file="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/tirtos/iar/stack/build_config.opt" -mv7M3 --code_state=16 -me -O4 --opt_for_speed=0 --include_path="C:/Users/Lucas Danrley/workspace_v11/simple_peripheral_cc1350lp_stack_FlashROM" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/examples/rtos/CC1350_LAUNCHXL/blestack/simple_peripheral/src/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/target/_common/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/hal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/osal/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/saddr" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/aes/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv/cc26xx" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/services/src/nv" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/src/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/controller/cc26xx/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/npi/src" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/common/cc26xx/npi/stack" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/icall/inc" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/profiles/roles" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0" --include_path="C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/devices/cc13x0/inc" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-arm_20.2.5.LTS/include" --define=BLE_NO_SECURITY --define=CC13XX --define=CC13XXWARE --define=DeviceFamily_CC13X0 --define=DATA= --define=EXT_HAL_ASSERT --define=FLASH_ROM_BUILD --define=GATT_NO_CLIENT --define=INCLUDE_AES_DECRYPT --define=NEAR_FUNC= --define=OSAL_CBTIMER_NUM_TASKS=1 --define=OSAL_SNV=1 --define=POWER_SAVING --define=USE_ICALL --define=xDEBUG --define=xDEBUG_ENC --define=xDEBUG_GPIO --define=xDEBUG_SW_TRACE --define=xTESTMODES -g --c99 --gcc --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="Startup/rom_jt.d_raw" --obj_directory="Startup" "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom/rom_jt.c"
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
Finished building: "C:/ti/simplelink_cc13x0_sdk_4_20_00_05/source/ti/blestack/rom/rom_jt.c"

makefile:181: recipe for target 'all' failed

**** Build Finished ****

  • On the side: Do you plan only to run BLE? If so, look into one of the devices in the CC26xx family. Do you plan to use BLE + sub1GHz: Look into the CC1352 to get sufficient flash size to run both. 

  • Hi Lucas,

    I've reproduced your issue. There seems to be a problem in the osal.c file which is located inside the OSAL directory in the project. You can use CCS to point directly to the error, by double clicking the error in the Problems tab (normally located bottom right in CCS).

    This will open the file and point to the error. In this particular case, the error is a missing argument when making a call to ltoa().

    A temporary fix would be to change line 381 from this:

      return ( (unsigned char*)ltoa( l, (char *)buf ) );
    

    To this:

      return ( (unsigned char*)ltoa( l, (char *)buf, radix ) );

    Try that and let me know if it builds. I'll inform the appropriate team about this, so that they can fix it.

    BR,
    Andres

  • Hi Lucas,

    An update on the issue that you are facing. This is related to the CCS version you are using (i.e. 10.4.0). The release notes of the 4.20 SDK specify that it was tested using CCS 9.1, which uses an older version of the TI ARM compiler.

    If you want to use CCS 10.4, you need to download the older TI ARM compiler.

    You can find it here:

    www.ti.com/.../ARM-CGT

    This page shows three possible download options (CLANG, CGT-19, and CGT-18). You should download CGT-18.

    BR,
    Andres