This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v3.3 cannot connect to DSP QQ2812

Does someone use DSP 2812,? Please help me!

I do like the instruction in user manual but CCS doesn't connect. Instruction says:

open Setup CSSv3.3, select F2812 XDS510 Emulator> Properties>Auto-generate board data file with extra configuration file> Browse file Blackhawk.cfg>Next> Value 0x0>Finish. Save and start CCS3.3

On CCS3.3. Debug>Connect> error pop-up
Error connecting to the target:
Error 0x80000240/-118
Fatal Error during: Initialization, OCS,
This error was generated by TI's USCIF driver.

Sometimes, error is:
Error connecting to the target:
Error 0x80000200/-1047
Fatal Error during: OCS,
PTI_ERR_EMU_CLOSE Error Occured at 0x00000000

I/O Port = 0

(I don't have blackhawk.cfg files, so I select some different .cfg file from blackhawk)

I don't understand, I installed usb driver (EZ-USB 68013). Can someone help me? Does someone have CD rom?