our project use the chip of C6713 and CCS3.3. Recently we want to use CCS4(bios 5.41) instead. the project is built and compiled OK, but the RTDX(log and cpu graph) can't work like this:
"Error: An error occurred connecting to Channel Server. Make sure this target supports tracing and it's connected. Native error message: "Channel server creation failed."
1. what's the reason, is it because 6713 is an old chip when is not supported?
2. if i only use bios5.41 with out RTSC, does the CPP supported in CCS4? what cpp library is provided by CCS? it will be good if u can provide some documents links.
thanks!