I have CCSv4.2.3.00004 microprocessor node locked single user liscence. running on windows xp SP3 and am using an Stellaris BD-ICDI-B to connect to the IDM-L35 but every time I try to debug I get:
CORTEX_M3_0: Error connecting to the target: Frequency is out of range.
I have the target connection setup as Stellaris In-Circuit Debug Interface and the board selected as a Stellaris LM3S1958.
I have the 10 position debug cable going from the ICDI to the IDM-L35. If I press the reset button on the ICDI the IDM-L35 resets.
Contents of target config file:
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Stellaris In-Circuit Debug Interface_0">
<instance XML_version="1.2" desc="Stellaris In-Circuit Debug Interface_0" href="connections\Stellaris_ICDI_Connection.xml" id="Stellaris In-Circuit Debug Interface_0" xml="Stellaris_ICDI_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Stellaris In-Circuit Debug Interface_0">
<instance XML_version="1.2" href="drivers\stellaris_cs_dap.xml" id="drivers" xml="stellaris_cs_dap.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers\stellaris_cortex_m3.xml" id="drivers" xml="stellaris_cortex_m3.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="Stellaris LM3S1958_0" href="Devices\lm3s1958.xml" id="Stellaris LM3S1958_0" xml="lm3s1958.xml" xmlpath="Devices"/>
</platform>
</connection>
</configuration>
</configurations>