This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: CCS3.x to CCS12 migration - BIOS issue

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: SYSBIOS, UNIFLASH, SYSCONFIG

Hi,

As a follow-up to this question, I have issues with the linking of the project.

>> Compilation failure
makefile:202: recipe for target 'Monodouble.out' failed
4F0}: cannot stat 'C:\Users\A0564~1.THU\AppData\Local\Temp\76A143F2-0B79-4E2C-AEF7-20D4C9A494F0': No such file or directory
error #10008-D: cannot find file "biosi.a28l"
gmake[1]: *** [Monodouble.out] Error 1
gmake: *** [all] Error 2
makefile:198: recipe for target 'all' failed

It seems that there is a file that should be generated in a temporary folder, and isn't. Or at least, that's my understanding of the issue.

The project is configured with DSP/BIOS 5.42.2.10.

Thanks in advance, 

Best regards,

Adrien