This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: Sysconfig CLB Tile Design settings reset when changing tile Name?

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE, LAUNCHXL-F28P65X

I have been using sysconfig (version 1.19.0.3426) in CCS (version 12.6.0.00008) and I have come across some unexpected behaviour in the Configurable Logic Block > Tile Design window.

When changing the Name entry of an existing Tile in the tile design window, existing settings for that tile are cleared to defaults.

Original display:

..after changing tile name only:

Is this expected behaviour?

It would be useful to be able to adjust the name of the tile without having to go through and re-input all the tile settings.

Thanks,
Alex