This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2650: cc2650 and associated ti dev platforms i.e. launch and sensor tag

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650, CC1310

Tool/software:

using plain CCS not rfstudio

looked everywhere (probably not everywhere but spent hours)

- missing the code for the out of the box demo

- missing any kind of examples

Thank you

  • Hello Ioana Panu,

    I hope you are doing well. On TI.com in the CC2650's software development section has the available software packages:

    Thanks,
    Alex F

  • Thank you for fast reply

    That did not help too much. it is a the BLE stack that presumably supports cc2650/cc1310 family. it is the setup for windows platform which will not work on any other platform. On top of that there is no easy way to unpack a upx file to extract the sources I might be interested in.

    It seems ti is forcing us, now, to either switch to the cloud based ide, which does not have what I was looking for, or move to windows platform.

    No offence but it can be seen that the clowd platform is linux based on theia server.

    Anyhow I have to move, most likely, to another vendor. 

    Thank you

  • Hello Ioana Panu,

    Just to confirm here, the example you need is in the BLE stack (something like project_zero?), and you do not use Windows (so the CC2650 Windows example will not work).

    I assume you have already referenced CC2650 LaunchPad, but if you are doing new BLE development we would recommend other devices currently. 

    Thanks,
    Alex F