This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP debugging in Netra using CCS not working.

Hi,

We are getting the following output in the console when tried to connect DSP in DM8168 through CCS.

This started happening after adding couple of more software modules in DSP.


[C674X_0] Invalid CIO command (136) in the CIO buffer at address (0x90a412d0) was not recognized. Please check the device and program memory maps.
[C674X_0] Invalid CIO command (136) in the CIO buffer at address (0x90a412d0) was not recognized. Please check the device and program memory maps.
[C674X_0] Invalid CIO command (136) in the CIO buffer at address (0x90a412d0) was not recognized. Please check the device and program memory maps.

 

Can someone point out the reason for the same?

How can we address the issue?

 

Thanks and Regards,

Nitish James